Safety in Mining Through Progress

The mining industry remains a field that is notoriously unforgiving. From harsh environments to rigorous demands on the crew and machinery, this environment is full of inherent risks. Mitigating these risks should be at the forefront of every operator’s mind, and there are plenty of options to find the best solutions for your operation. Technical innovations like soft braking systems and modern advancements in monitoring software have made safety around critical processing and transportation equipment easier than ever to implement. These systems work together not only to enhance safety on the jobsite but also boost productivity and decrease unplanned downtime.

Soft Braking Evolution in the Industry

Over the years, the constant strive for improvement in operational safety has led to some interesting technological advancements. One notable example is the introduction of controlled braking into the conveying technology on these mining sites. These systems helped modulate and control the torque spikes to enhance safety and extend the lifetime of the systems impacted by these heavy loads.

This implementation started to expand across the industry, and notable companies like Svendborg Brakes™ further developed this idea, moving towards more ways to monitor and customize these safety options. Advancements in PID type control with the hopes of giving operators even more control over low-torque, low-volume, and places where optimizing oil flow were important leading to a steep decline in catastrophic brake failures.

Smart Monitoring Systems on Your Operation

With advanced mechanical upgrades in the field comes technology to complement it. The inclusion of smart systems on your mining operation, while being a great benefit to safety, also gives you the opportunity to incorporate several monitoring systems to further increase efficiency and uptime while on the site.

One of these systems relates back to Svendborg’s SOBO iQ, which allows operators the ability to see real-time feedback from their machinery. There are similarities with other monitoring systems, but among all the differences, the opportunity to diagnose and prevent unplanned downtime remains at the height of this technology’s focus.

Specific use cases could include monitoring your braking systems’ function and pressure during operation. By analyzing the pressure curves and readouts, the opportunity to catch any irregularities is heavily increased. By noticing spikes or pressure differences across consistent monitoring, you can plan downtime to repair or inspect these systems, which may have escalated to failure and longer downtime, or worse, if they went unnoticed.

This is just one of the many ways to utilize this kind of technology. Monitoring systems and the teams behind them can create customized services that can measure many kinds of technical data specific to your operation. By having the freedom and opportunity to tailor what is monitored based on a multitude of factors, you can ensure that not only is the machinery itself in good hands, but proactive measures are also being taken to ensure the longevity and productivity of these operations.

Security at the Forefront of Innovation

Mining operations constantly measure, and store personalized sensitive data. By incorporating outside monitoring, the concern of having your operation's sensitive information stolen isn’t unreasonable. However, many monitoring systems, like SOBO iQ, for example, are NIS2 compliant and work with your operation to ensure the safe and secure transfer of real-time data. Working together with teams of specialists off-site helps your team focus on the crucial operation of machinery while off-loading stressful data analysis to teams with years of experience identifying and diagnosing irregularities in the data.

The mechanical benefits of the SOBO iQ system are clear, and having a control system that gets real-time customized feedback only adds to its benefit. By working with trusted experts, mining operators can gain valuable insights from their monitoring systems, enhancing uptime and operational efficiency. The SOBO iQ system's ability to provide detailed data and predictive maintenance ensures that operators can confidently manage their equipment and maintain safety standards.

Strive to Improve

As the world pushes forward, so can your operation. By staying on top of recent technical and mechanical improvements, you will always be at the forefront of safety innovation. The more we can adapt to moving forward, the greater the odds of favorable personnel and business risk-mitigation outcomes. When it comes to systems that can prevent catastrophes and unplanned downtime, no shortcuts should be taken. By ensuring you have the most updated safety features alongside monitoring software that can analyze data and catch even the smallest irregularities, you lead the way in providing the best working conditions for those at your operation.

Want to connect? Let’s introduce you to a mining industry expert here:
bsfi_3000_ds
Enhancing mining conveyor safety with intelligent soft braking systems at Global Mining Review