The Importance of Safety in the Mining Industry
The rugged, high-stakes environment of the mining industry requires safety to be non-optional. Every piece of equipment, every process, and every decision must come together to ensure the livelihood of our work force is preserved and operational excellence is achieved. From conveyor systems to hoists and grinding mills, these critical components play a large part in providing essential raw materials to the global economy. One crucial element that plays a vital role to all of these sectors, however, are the braking systems of these heavy applications.
The Critical Role of Brakes in Mine Safety
Brakes are a fundamental component in various mining applications, playing a crucial role in ensuring the safety of operations. Some key examples of how brakes are properly utilized within the industry include:
- Conveyors: Conveyor systems are used to transport materials over long distances within a mine. Brakes are essential for controlling the speed of conveyor belts, preventing overloading and mechanical failures that could lead to accidents. Effective braking systems ensure that conveyors can be stopped quickly in emergencies, reducing the risk of injury to workers.
- Hoists: Hoists are used to lift and lower materials and personnel in mines. Reliable braking systems are critical for hoists to prevent uncontrolled descent, which could result in severe accidents. Advanced braking technologies, such as fail-safe brakes, ensure that hoists can stop safely even in the event of a power failure.
- Grinding Mills: Grinding mills are used to crush and grind ore into smaller particles. Brakes are vital for controlling the rotational speed of the mills, ensuring safe operation. In case of an emergency, brakes can quickly stop the mills, preventing potential hazards such as mechanical failures or explosions.
Application Considerations and Technological Advancements
There are many factors reviewed when designing and selecting a braking system – the torque applied when braking, location and orientation of the equipment, and operating conditions to name a few. However, braking is not as simple and on or off, often it requires accurate speed modulation and contingencies for power loss, speed signal errors, or mechanical failures. Innovations in smart braking technologies have aided significantly in managing increased demands, detecting and monitoring equipment wear and status, and responding to changes in system resource availability.
A good example of these safety features being considered can be seen in Regal Rexnord’s emphasis in advanced braking solutions from one of its brands, Svendborg Brakes. Their innovative braking solutions incorporate features like hydraulic releases and soft braking, significantly reducing wear and tear while ensuring precise control. Having these systems installed and in mind ensure proactive steps are being taken to significantly reduce the chance of injury on the work site.
SOBO® (SOft Braking Option) iQ’s deployment by Svendborg Brakes has continued to show immense improvements towards the safety of conveyor systems. Integrating advanced braking algorithms with state-of-the-art hydraulic technology is a great step towards ensuring the safety of those on the jobsite. Designed to mitigate uncontrolled loads and prevent catastrophic failures, SOBO iQ’s braking protocols ensure smooth and controlled deceleration and the intelligent feedback mechanisms optimize braking force dynamically enable safe and reliable operation under various load conditions.
Pursuing Safety in Your Mine
Incorporating a design partner like Regal Rexnord’s powertrain solutions team into a new project or existing refurbishment can aid in identifying the variables needed for consideration and resources available to combat risk. This inclusion can pay dividends in both upfront design efforts and long-term risk prevention. The cost of downtime due to poor system selection can be immense, and a preventable injury or fatality would be catastrophic.
While the mining industry has made progress in improving safety standards, the journey towards a completely safe working environment is ongoing. Continuous innovation and adherence to safety protocols are imperative. Brakes, as a critical safety component, exemplify how targeted improvements in equipment can significantly enhance the safety of mining operations, and by prioritizing safety, the mining industry can protect its most valuable asset—its workforce.
Regal Rexnord’s 30,000 associates around the world help create a better tomorrow by providing sustainable solutions that power, transmit, and control motion. The Company’s electric motors and air moving subsystems provide the power to create motion. A portfolio of highly engineered power transmission components and subsystems efficiently transmit motion to power industrial applications. Regal Rexnord’s automation offering is comprised of controls, actuators, drives, and precision motors that control motion in applications ranging from factory automation to providing precision control in surgical tools.
The Company’s end markets benefit from meaningful secular demand tailwinds, and include factory automation, food & beverage, aerospace, medical, data center, warehouse, alternative energy, residential and commercial buildings, general industrial, construction, metals and mining, and agriculture.
Regal Rexnord is comprised of three operating segments: Industrial Powertrain Solutions, Power Efficiency Solutions, and Automation & Motion Control. Regal Rexnord is headquartered in Milwaukee, Wisconsin and has manufacturing, sales, and service facilities worldwide. For more information, visit RegalRexnord.com.